Manufacturing companies prioritize high reliability, which refers to a low failure rate and long lifespan, as their primary requirement for industrial robots. The second focus is on high performance, including factors such as efficiency, beat rate, and precision. Additionally, the ability to provide flexibility and expandability is also considered advantageous. In response to these priorities, ROKAE Robotics has conducted extensive case studies and developed new industrial robot products, namely the NB12 and NB25 series. These products have been successfully implemented in large-scale applications and have received widespread acclaim from customers due to their high reliability.
High-Reliability Industrial Robots
At the onset of 2023, ROKAE Robotics has surpassed the MTBF (Mean Time Between Failure) certification benchmark of 80,000 hours, thereby demonstrating the exceptional performance of their products in terms of reliability.
This high level of reliability is further evident in ROKAE Robotics' two series of industrial robots, namely NB12 and NB25. These robots have been equipped with upgraded dynamic and static seals, ensuring a high level of protection at IP65 or above. Notably, the NB12 series possesses an IP67 rating, enabling it to maintain stable performance even in harsh environments characterized by humidity and spraying. Additionally, both the components and the entire robot have undergone rigorous quality inspections and have obtained various internationally recognized certifications, including CE, CR, KCS, and EAC. Consequently, the NB25 and NB25 series robots are also renowned for their reliability in practical application scenarios.
In practical application scenarios, the NB12 and NB25 models have been optimized to meet specific requirements. The NB12 series, for instance, incorporates cast aluminum components, resulting in a 30% reduction in weight compared to similar products. Additionally, the motors and cables are integrated into the body, leading to a more compact structure and a 47% reduction in size compared to products of the same level. The mounting options of front, side, and inverted mounting offer flexibility in narrow spaces. Moreover, the single-axis rotational range is expanded, minimizing blind spots and ensuring comprehensive coverage of the robot's work. Consequently, these features make the NB12 and NB25 models suitable for a wide range of applications involving small payload robots.
The NB25 series of robots has been designed to cater to a wide range of application requirements in various scenarios. As a result, the load capacity of the NB25 series has been increased by an average of 25% compared to its previous generation. This improvement has been achieved through the optimization of trajectory planning algorithms, enabling the robots to perform more efficiently and support the motion characteristics of high inertia loads. Consequently, the NB25 series is particularly suitable for scenarios involving large inertia, large-size loads, and high-speed operations. Additionally, the NB25 series offers a longer reach within its class, ranging from 1617mm to 2110mm, allowing for flexible deployment in narrow spaces. Furthermore, the NB25 series boasts a longer boom span within its class, covering the same range of 1617mm to 2110mm. This feature enables the robots to easily accommodate a wider range of operational requirements.
ROKAE Robotics has established itself as a leading force in the industry, renowned for its exceptional reliability and performance. This reputation is attributed to the company's robust technological innovation capability, efficient product development system, and stringent quality management system. As a result, ROKAE Robotics has successfully expanded its business presence across numerous regions, including Europe, America, East Asia, and Southeast Asia, encompassing over a hundred territories.
High-Precision and High-Efficiency Industrial Robots
The NB12 series incorporates ROKAE's proprietary xCore control system, which utilizes OptiMotion and TrueMotion dual technology. This integration enhances the speed of operation while ensuring a high level of accuracy, as evidenced by its repeatability of ±0.03mm. Additionally, the NB12 series offers a 20% increase in operation speed, making it suitable for fast-paced and high-precision production requirements. Consequently, the implementation of this technology significantly enhances production capacity.
The NB25 series is a versatile product designed to cater to various application needs in different settings. It not only enhances operational speed but also ensures reliability, thereby contributing to the optimization of production efficiency. An example of this is the NB25-12/2.1, a specialized robot specifically designed for photovoltaic layout tasks. This robot not only significantly reduces the time required for each layout cycle to less than 5 seconds but also executes smoother and more fluid motion paths. These features make it highly suitable for high-efficiency scenarios, providing adequate safeguards for overall production capacity during layout processes.
ROKAE Robotics has achieved a high level of international prominence largely due to its research and development efforts in controller technology, enabling them to master the core technology of high-performance control systems. The controller, as one of the three essential components of a robot, serves as its "brain". In fact, the performance disparity between domestic and foreign robots can be attributed to the overall gap in controller technology. Leading robotics companies typically emphasize the use of self-produced and self-utilized controllers to showcase their products. This is because only a controller developed in-house can fully align with their specific robotic products and unleash their maximum performance potential. Consequently, the future success in the robotics market will inevitably be attained by companies that possess expertise in core control technology, and ROKAE Robotics undoubtedly possesses an inherent advantage in this regard.
Conclusion
ROKAE Robotics has positioned itself as a pioneering technology company, with a strong focus on innovation and enterprise development. The company has successfully mastered various technological aspects, including algorithms and flexible force control, which serve as the foundation for their high-performance robot control system. Additionally, ROKAE Robotics has independently developed highly integrated modular joints and other core components, enabling them to create a comprehensive product line consisting of industrial robots and collaborative robots, ranging from 3kg to 220kg. These products are designed to provide innovative, efficient, and competitive smart manufacturing solutions that cater to the diverse needs of customers. By implementing these solutions, enterprises can achieve cost reduction and improved efficiency, while also contributing to intellectual innovation within the industry.