Introduction
1. How to achieve both speed and accuracy in the photovoltaic industry, where single-line capacity is getting higher and higher?
2. How to meet the demand for a super-large size layout, which requires a robot with a larger reach to achieve compatibility?
3. How to achieve the true meaning of "clear vision" with the strong cooperation between vision system and robot?
Customers and market demand are the sources of innovation for enterprises. Listening to customers' voices and continuously launching products and services that meet customers' needs is the embodiment of ROKAE's "customer-centric" service consciousness.
In the process of cultivating the photovoltaic industry, ROKAE found that the above-mentioned problems have become a challenge for our customers. For this reason, we launched a new generation of solar panel lay-up robot NB25-12/2.1 based on the ROKAE industrial product platform and market-oriented, providing one-stop robot solutions for the intelligent industrial upgrading of the photovoltaic industry.
01 High speed + high precision, to create the industry's top production capacity
Customer pain points
"The single production line in the photovoltaic industry requires increasingly high production capacity, and the robot is running at a fast pace, requiring precision in the face of increasing speed. The robot's high-speed operation often causes the frame to shake, which in turn affects the overall accuracy of the lay-up, so we have to find ways to strengthen the equipment." The person in charge of the customer's automation talked about how, for PV companies, high speed and high precision of products are necessary factors to ensure their core competitiveness in the fierce market competition.
Solutions
Robot Optimization
The special design of high inertia and high rigidity of ROKAE's solar panel lay-up robots can give the robots faster movement speed in each axis and ensure the reliability during long operation, laying the foundation for achieving "high speed + high precision".
System upgrade
By adopting the new xCore control system developed by ROKAE, the speed of ROKAE's solar panel lay-up robots is easily reduced to less than 5 seconds/cycle, and the motion trajectory is even smoother, fully satisfying high-precision applications and guaranteeing the overall accuracy of lay-up.
02 Large reach + high payload, compatible with the full range of lay-up needs
Customer pain points
"The existing robot has a reach of only 2 meters, which is often overstretched when facing the oversized lay-up needs of end customers. As a result, we had to adjust the machine's mechanical mechanism to meet the new demand. This not only increased the workload but also the design and manufacturing costs and the corresponding riskiness." So said the head of the customer's delivery chain in an interview.
Solutions
Large Reach
The reach of ROKAE's solar panel lay-up robot was extended from 2013 mm to 2110 mm, and the advantages of the large reach were maximized by optimizing the mechanical structure.
High Payload
The load capacity of the robot is increased from 10 kg to 12 kg, which is able to cope with the load demand during the upgrade of the lay-up machine.
03 Customized vision system, more efficient production, more convenient use
Customer pain points
"Driven by the demand for flexible and intelligent production lines, vision systems and robots are becoming increasingly sophisticated. However, the current conventional integrated solutions not only still have technical barriers, but also make the subsequent commissioning and service more difficult." Customer after-sales service personnel said.
Solutions
One-stop solution
Relying on the perfect solution system, ROKAE not only provides customers with robots but also develops a whole set of customized lay-up vision solutions to meet customers' needs. By upgrading the integrated solution of "robot + vision" to a one-stop solution, ROKAE has achieved the true meaning of "clear vision" and also solved the worries of customers' on-site commissioning and service.
As the demand for automation in the PV industry continues to rise, ROKAE relies on its excellent robotics portfolio and its ability to plan and implement intelligent manufacturing solutions to launch new robots for PV plate-making, providing "efficient tools" for the overall upgrade of intelligent manufacturing in the PV industry.
In the future, ROKAE will continue to explore the application process of the PV industry chain, and continue to provide one-stop robot solutions for the industry to promote the early realization of the goal of "carbon peak" and "carbon neutrality".